MTN6710-0102S / MTN6810-0102 / MTN6805-0008

Failure and Download Behavior

You can enable this function individually for each drive. The behavior of the drive in the case of a bus voltage failure / bus voltage recovery and application download is defined.


NOTICE
Behavior of blind and shutter outputs has changed.
The Dimmer Master does not have enough power to move all blind and shutter channels into position or to move them up or down. Only the following options are available here:
  • Relay state after bus voltage failure: No reaction
  • Relay state after bus voltage failure: Stop

Ext. 1/2

Output 1+2 / 3+4 / 5+6 / 7+8

-Blind / roller shutter

-Safety and alarm settings

Failure and download behavior

Failure and download behavior

Disabled

Enabled

Relay state after bus voltage failure

No reaction

Stop

Relay state after bus voltage recovery

Stop

Up

Down

Move to position

As before bus voltage failure

   

Height position at bus voltage recovery in %

0 (0-100)

   

Slat position at bus voltage recovery in %

0 (0-100)

   

Relay state at end of download

Stop

Up

Down

Move to position

As before download

   

Height position at end of download in %

0 (0-100)

   

Slat position at end of download in %

0 (0-100)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?