MTN6710-0102S / MTN6810-0102 / MTN6805-0008

Different Running Times for Up and Down

If the parameter Use same time for up and down is deactivated, different running times can be set for up and down. The Running time: Up should be parameterized slightly longer so that the end stops are always reached, even in the case of low temperatures or a heavy blind / roller shutter.

Ext. 1/2

Output 1+2 / 3+4 / 5+6 / 7+8

Blind/roller shutter

Express settings for blind/roller shutter

 

Blind control / roller shutter control

 

Use same time for up and down

No

 
   

Up time (5s...99:59.9 min)

02:00.0

   

Down time(5s...99:59.9 min)

02:00.0

The Running time: Up should be parameterized slightly longer so that the end stops are always reached, even in the case of low temperatures or a heavy blind / roller shutter.

This type of running time allowance should be taken into account due to the physical fact that drives take longer for upward movements than for downward movements due to the effect of gravity on the blind / roller shutter. Since this time deviation can be very short, you have to execute multiple movements to become aware of this behavior. It is useful to move the drive from 10% to 90% and back to 10% several times. If you notice that the drive does not completely reach the upper end position after these movements, you can increase the “Running time: Up”.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?