MTN6710-0102S / MTN6810-0102 / MTN6805-0008

Defined Number of Blinking Intervals

You can reduce the blinking intervals to a defined number (0...255) to protect the relay.

With “0”, the number of blinking intervals is unlimited, so the relay blinks permanently.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?