MTN6710-0102S / MTN6810-0102 / MTN6805-0008

Time Extension

If you want to restart the staircase lighting time before it has elapsed or add up the staircase lighting time, you must select the staircase lighting time Retriggerable or Retriggerable and adding or Retriggerable to the higher value. The staircase lighting time is then restarted or added using another “1” telegram.


Time extension = Retriggerable

Once a new telegram with the object value “1” has been received, the staircase lighting time is restarted.


Time extension = Retriggeable and adding

Once one or more new telegrams with the object value “1” have been received, the staircase lighting time is added to the previous staircase lighting time. The number of additions can be set. You can parameterize a maximum of 5 additions of the staircase lighting time.

For example, you can add up the staircase lighting time by pressing a separate button several times.


Time extension = Retriggerable to the higher value (only for staircase lighting time = variable)

Once a new telegram has been received, the staircase lighting time is restarted with the higher value.


Time extension = Not retriggerable

However, if the staircase lighting time is not retriggerable, the relay will switch off at exactly the moment the time elapses.

If the Manual switching off function is activated, the staircase timer can be ended with a “0” telegram.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?