MTN6710-0102S / MTN6810-0102 / MTN6805-0008

Additional Start-up Time on Opening the Slat (for Blind only)

Some types of blinds require an additional start-up supplement before the first reaction of the slats when opening the slats due to the tensioning and releasing of the slat straps. This depends on the current slat position. The following parameters can be used to set a start-up supplement for the upper and lower slat positions.

Ext. 1/2

Output 1+2 / 3+4 / 5+6 / 7+8

-Blind/roller shutter

Extended drive timing

-Extended drive timing

Additional startup time when opening slat downwards (0...255, unit = 10 ms)

0

   

Additional startup time when opening slat upwards (0...255, unit = 10 ms)

0

With these parameters for Additional startup time when opening slat downwards, set the start-up delay for an upward movement until the slat is rotated when the slats are in the open position (0%) (the previous blind movement was an upward motion).


Additional startup time when opening slat upwards: the start-up delay until the slat is rotated, which you define here, is always taken into account when opening the blind if the slat is in the closed position (100%) (the previous blind movement was a downward movement).

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?