MTN6710-0102S / MTN6810-0102 / MTN6805-0008

Type of Delay

Delay times can be parametrized for each channel. You can use parameters to define the set delays as Retriggerable or Not retriggerable. In the case of a retriggerable on-delay, the delay time is restarted when a "1" telegram is received. In the case of retriggerable off-delays, the delay time is restarted when a "0" telegram is received.


Retriggerable on-delay (“1” telegram)


Retriggerable off-delay (“0” telegram)

Moreover, for the off-delay, you can also select Retriggerable and adding. The delay time is added when the same telegram value is received, e.g., using a separate button. You can define the maximum number of additions.

In the case of not retriggerable delays, by contrast, the relay will switch off at exactly the moment the time elapses.


Not retriggerable on-delay


Not retriggerable off-delay

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?