Group Objects of Automatic Mode Lock
|
No. |
Name |
Object function |
Length |
Behavior |
Data Type |
|---|---|---|---|---|---|
|
152 |
Extension Output 1+2 name of the channel |
Lock of automatic mode |
1 bit |
Received |
1.003 Enable |
|
160 |
Extension Output 1+2 name of the channel |
Feedback for automatic mode |
1 bit |
Sending |
1.003 Enable |
Depending on the setting, the automatic locking is activated or deactivated when a new telegram value is received:
-
“Automatic locking” = “at object value 0”
If “Automatic locking” = “0”: automatic locking is active.
If “Automatic locking” = “1”: automatic locking is inactive. -
“Automatic locking” = “at object value 1”
If “Automatic locking” = “0”: automatic locking is inactive.
If “Automatic locking” = “1”: automatic locking is active.
In addition, you can set the behavior of the drive to the end of automatic locking.
Furthermore, you can separately define the response of automatic control on receiving a manual control telegram.