Output Behavior after Bus Voltage Failure
If the bus voltage falls below 18 V, the output can be switched to a parametrized state. The output can be defined as either Switch off or Switch on at selectable brightness, or remain in the state it had before the failure (No reaction). At the same time, the current state of the output is saved in the device.
Possible settings:
-
No reaction
The output channel remains at its current brightness value. If time functions (staircase lighting time function, on-delay, off-delay) are currently active, they are canceled. -
Switch Off
The output channel is switched off. -
Switch on at selectable brightness
The initial brightness is determined by another parameter. The selectable brightness can be set between 1% and 100%.
NOTICE |
---|
Behavior of blind and shutter outputs has changed.
The Dimmer Master does not have enough power to move all
blind and shutter channels into position or to move them up or down.
Only the following options are available here:
|