Group Objects for Express Settings – Blind/Roller Shutter
|
No. |
Name |
Object function |
Length |
Behavior |
Data Type |
|---|---|---|---|---|---|
|
143 |
Extension Output 1+2 name of the channel |
Movement in manual mode |
1 bit |
Received |
1.008 Up/Down |
|
144 |
Extension Output 1+2 name of the channel |
Stop/step in manual mode (blind) |
1 bit |
Received |
1.007 Step |
|
144 |
Extension Output 1+2 name of the channel |
Stop in manual mode (roller shutter) |
1 bit |
Received |
1.007 Step |
|
145 |
Extension Output 1+2 name of the channel |
Height position in manual mode |
1 byte |
Received |
5.001 Percent (0...100%) |
|
146 |
Extension Output 1+2 name of the channel |
Slat position in manual mode (blind) |
1 byte |
Received |
5.001 Percent (0...100%) |
|
158 |
Extension Output 1+2 name of the channel |
Feedback for height |
1 byte |
Sending |
5.001 Percent (0...100%) |
|
159 |
Extension Output 1+2 name of the channel |
Feedback for slat (blind) |
1 byte |
Sending |
5.001 Percent (0...100%) |
|
163 |
Extension Output 1+2 name of the channel |
Feedback for moving |
1 bit |
Sending |
1.010 Start/Stop |
|
164 |
Extension Output 1+2 name of the channel |
Feedback for last direction |
1 bit |
Sending |
1.008 Up/Down |