Group Objects of Status Response for Blind/Roller Shutter
|
No. |
Name |
Object function |
Length |
Behavior |
Data Type |
|---|---|---|---|---|---|
|
158 |
Extension Output 1+2 name of the channel |
Feedback for height |
1 byte |
Sending |
5.001 Percent (0...100%) |
|
159 |
Extension Output 1+2 name of the channel |
Feedback for slat (blind) |
1 byte |
Sending |
5.001 Percent (0...100%) |
|
163 |
Extension Output 1+2 name of the channel |
Feedback for moving |
1 bit |
Sending |
1.010 Start/Stop |
|
164 |
Extension Output 1+2 name of the channel |
Feedback for last direction |
1 bit |
Sending |
1.008 Up/Down |