Group Objects of Automatic Mode for Blind/Roller Shutter
|
No. |
Name |
Object function |
Length |
Behavior |
Data Type |
|---|---|---|---|---|---|
|
148 |
Extension Output 1+2 name of the channel |
Movement in automatic mode |
1 bit |
Received |
1.008 Up/Down |
|
149 |
Extension Output 1+2 name of the channel |
Stop/step in automatic mode (blind) |
1 bit |
Received |
1.007 Step |
|
149 |
Extension Output 1+2 name of the channel |
Stop in automatic mode (roller shutter) |
1 bit |
Received |
1.007 Step |
|
150 |
Extension Output 1+2 name of the channel |
Height position in automatic mode |
1 byte |
Received |
5.001 Percent (0...100%) |
|
151 |
Extension Output 1+2 name of the channel |
Slat position in automatic mode (blind) |
1 byte |
Received |
5.001 Percent (0...100%) |
The group objects for manual operation and automatic mode have equal priority. The drive always executes the command it received last on one of the objects.
Using parameter settings and objects, you can modify the operation of the two control options. You also have the possibility of defining the reciprocal influence of manual control and automatic control.