Group Objects of Locking Function
|
No. |
Name |
Object function |
Length |
Behavior |
Data Type |
|---|---|---|---|---|---|
|
153 |
Extension Output 1+2 name of the channel |
Lock |
1 bit |
Received |
1.003 Enable |
|
161 |
Extension Output 1+2 name of the channel |
Feedback for drive locking |
1 bit |
Sending |
1.003 Enable |
If the locking object receives a telegram with the object value that you set for the parameter Lock, all other functions for the channel are disabled. You can define the reaction using the parameter Behavior at start of locking.
If the locking object receives a telegram with the object value opposite of that for activation, the lock is canceled and the drive adopts the state that you defined in the parameter Behavior at end of locking.
The Feedback for drive locking object sends a “1” if the lock is active.
The Feedback for drive locking object sends a “0” if the lock is inactive.