MTN6710-0102S / MTN6810-0102 / MTN6805-0008

Priority

The reaction to the behavior set here for bus voltage recovery has a low priority.

If a function with a higher priority is activated for the drive directly after bus voltage recovery, the settings described below apply to these functions.

Relay states caused by higher-priority functions (higher-level function) take precedence over behavior after bus voltage recovery.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?