MTN6710-0102S / MTN6810-0102 / MTN6805-0008

Minimum Brightness

Faults such as flickering may occur at minimum brightness values. The brightness of the lamps may have fallen below the minimum value. In this case, increase the minimum dimming value.

If lamps can only be dimmed slightly, check whether the minimum dimming value has been set too high (range 1-25%).

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?