Device Safety
This parameter activates the central safety object.
For each channel, a channel parameter can be used to determine whether and how this channel should respond to the safety object. The object value for the device safety function can also be set.
The device then waits for a telegram from an external sender within the set cycle time. If such a telegram is not received within the monitoring time, it is then possible to decide for each channel what should happen.
Dimming: Safety Function Dimming
Switch: Safety Function Switching
Blind: Safety Function Blind
Roller shutter: Safety Function Roller Shutter
|
Extended settings |
Device safety |
||
|
Device safety |
At object value "1" At object value "0" |
||
|
Disabled |
|||
|
Cycle time surveillance for Safety object (0 ... 255, unit = 1 s, 0 = inactive) |
0 |
After enabling device safety function, the Safety group object appears.