MTN6710-0102S / MTN6810-0102 / MTN6805-0008

Object Values for Alarm

First select the object value that is to switch on the alarm function:

  • At object value “1”: object value “1” switches on the alarm function. If the object value “0” is received, the alarm function is switched off again.

  • At object value “0”: object value “0” switches on the alarm function. A telegram with the object value “1” deactivates the function again.


The alarm function is activated if the alarm object receives a telegram with the object value that you defined with the parameter Alarm. The reaction is defined by the parameter Behavior at start of alarm.

  • No reaction: Finish actual task.

  • Stop: The drive remains in its current position.

  • Up: The drive moves to the upper end position.

  • Down: The drive moves to the lower end position.

  • Move to position: The drive moves to the defined position for height and slat (for blind only).


Once the drive has performed the desired action, it remains in this position and cannot be operated while the alarm function is active. Only when a function with a higher priority becomes active will the reaction defined there be executed.

If the alarm object receives a telegram with the object value opposite of that for activation, the alarm function is canceled and the output relay adopts the state that you defined in the parameter Behavior at end of alarm.

  • No reaction: the drive remains in its current position.

  • Up: the drive moves to the upper end position.

  • Down: the drive moves to the lower end position.

  • Move to position prior alarm: the drive returns to the position it had before the alarm telegram.

  • Accept current automatic position: this setting is only useful if the automatic function is active. The drive moves to the last automatic position requested.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?