MTN6710-0102S / MTN6810-0102 / MTN6805-0008

Failure and Download Behavior

You can enable this function individually for each switching channel. The behavior of the switch output in the case of a bus voltage failure / bus voltage recovery and application download is defined.

Ext. 1/2 Output 1-8 -Switch: Switching

Failure and download behavior

– Safety and alarm settings

Failure and download behavior

Disabled

Enabled

 

Relay state after bus voltage failure

No reaction

Pressed

Released

   

Relay state after bus voltage recovery

As before bus voltage failure

Pressed

Released

   

Relay state at end of download

As before download

Pressed

Released

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?