MTN6710-0102S / MTN6810-0102 / MTN6805-0008

Operating Principle

A reference movement can be triggered by a telegram on the central calibration object or after a certain number of movements. After a reference movement has been triggered, the drive moves to the desired reference position (end position). If you have set both end positions as reference positions, the drive will move to the nearest end position, depending on its current position.

In order to ensure that the drive reliably reaches the desired end position, the actuator adds a running time allowance of 5% of the total running time to the calculated travel time for each reference movement.


NOTE: If a weather alarm or other higher-level function is activated during a calibrating function, the calibrating function is canceled and the higher-level function is executed.


Per channel:

Ext. 1/2

Output 1+2 / 3+4 / 5+6 / 7+8

-Blind/roller shutter

Calibration

-Automatic, Locking & Calibration settings

Calibration

Disabled

Enabled

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?