MTN6710-0102S / MTN6810-0102 / MTN6805-0008

Status Response

Ext. 1/2

Output 1+2 / 3+4 / 5+6 / 7+8

-Blind / roller shutter

Express settings for blind / roller shutter

 

Status of height

Enabled

Disabled

   

Status of slat (for blind only)

Enabled

Disabled

   

Status of moving

Enabled

Disabled

Each blind channel can provide different status responses, depending on how it is enabled. The status response group objects are available and can be disabled.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?