MTN6710-0102S / MTN6810-0102 / MTN6805-0008

Prewarnings

If you have activated Switch-OFF Prewarning for staircase timer then you can set a warning time as a period between 5 s and 255 s (= 4 min 15 s). This warning time determines how long the dimming-down procedure should last.


Staircase lighting time function with Switch-off Prewarning

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?