Group Objects for Switching Cycle Counter
If you enable the Switching cycle counter, group objects for each relay appear in the special object folder Switching cycle counter.
|
No. |
Name |
Object function |
Length |
Behavior |
Data Type |
|---|---|---|---|---|---|
|
39 |
Extension 1/2 Output # |
Switching cycle counter |
2 bytes |
Sends/Reads |
2 byte unsigned value |
By default only C-Flag and R-Flag are set to avoid high bus traffic.
The firmware checks the internal counters cyclically every 10 seconds. If the value changes, it is sent via the Switching cycle counter object.
You can read the actual values via group objects. If you want to get to know the values without reading, you have to set the T-Flag for the object.