MTN6710-0102S / MTN6810-0102 / MTN6805-0008

Defining Dependency between Automatic Function and Manual Control

You can use the following parameter to define the reaction of the automatic function on receiving a control telegram from the manual operating options (Movement in manual mode, Stop/step in manual mode, Height position in manual mode, Slat position in manual mode, and calling up scenes):

Ext. 1/2

Output 1+2 / 3+4 / 5+6 / 7+8

-Blind/roller shutter

Automatic, Locking & Calibration settings

-Automatic, Locking & Calibration settings

Automatic mode

   

Reaction in automatic mode on receipt of a manual object value

Automatic mode remains enabled

   

Automatic mode temporarily disabled

   

Deactivation time for automatic mode

1 min (1 min - 24 h)

Permanent deactivation of the automatic function can only be canceled by a telegram terminating automatic locking via the automatic locking object. The action you set in the parameter "Behavior on deactivating automatic locking via object" will be executed.

Once a temporary deactivation has elapsed, the drive remains in its current position until the next control telegram.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?