MTN6710-0102S / MTN6810-0102 / MTN6805-0008

Switch

To switch electrical loads, you can switch the channel function of the device to Switch mode.

General settings

Channel function Extension 1 / Extension 2 Output 1-8 Switch
   
Ext. 1/2
Output 1-8 -Switch: Switching
Express settings for switching

...

Express Settings for Switching

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?