MTN6710-0102S / MTN6810-0102 / MTN6805-0008

Energy Saving

The status LEDs of the channels on the master can be switched off automatically after a period of between 1 minute and 255 minutes. In this way, you do not illuminate the switch cabinet unnecessarily. Pressing a button reactivates the LEDs for the preset time.

Extended settings

Energy saving

 
 

LEDs on the device can be set to standby after (0...255, unit = 1 min, 0 = always on)

0

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?