MTN6710-0102S / MTN6810-0102 / MTN6805-0008

Value Object Switches Channel

You can establish the settings for switching the dimming output on and off via the value dimming function using a parameter.

Master/Ext. 1/2 Output 1-2: Dimming

Express settings for dimming

 

Value object switches channel

Not

Only on

Only Off

On and Off


Possible settings

  • Not
    This parameter setting prevents switching, i.e. the channel remains at the current value.

  • Only On
    The output channel can be switched on by value telegrams. If it is switched on and the value object receives the value 0%, the output remains switched on at the value Minimum brightness in %.

  • Only Off
    The output channel cannot be switched on by value telegrams. If it is switched on and the value object receives the value 0%, the output is switched off.

  • On and Off
    The output channel can be switched on by value telegrams. If it is switched on and the value object receives the value 0%, the output is switched off.

NOTE: The setting Always start at 50% brightness (ESL/CFL) for compact fluorescent lamps influences the switch-ON behavior (Always Start at 50% Brightness (ESL/CFL)).

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?