MTN6710-0102S / MTN6810-0102 / MTN6805-0008

Switch-ON Behavior (via Switch Object)

Master/Ext. 1/2 Output 1-2: Dimming

Express settings for dimming

 

Switch-ON behavior (via switch object)

Max. brightness

Last brightness (Memory)

Selectable brightness

 

Initial brightness in %

100 (1-100)

Possible settings:

  • Max. brightness
    The output channel is set to the value which you have set in the parameter (B) Maximum brightness in %.

  • Selectable brightness
    For this value, an additional parameter appears. Initial brightness in %
    The output is switched to the set initial brightness with a “1” telegram. The value of the initial brightness should not exceed the maximum dimming value. The maximum output brightness is always limited by the maximum dimming value. Higher values for the initial brightness are ignored. If the selected initial brightness is less than the minimum dimming value, this value is also ignored. In this case, the minimum dimming value is used as the starting value.

  • Last brightness (memory)
    After a “1” telegram, the output is reset to the last brightness value it had before switching off.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?