MTN6710-0102S / MTN6810-0102 / MTN6805-0008

Overwrite Scene Values during Download

Ext. 1/2 Output 1-8 -Switch: Switching

Scene settings

 
Scenes settings

Overwrite scene values of actuator during download

Enabled

Disabled

If you have enabled the parameter “Overwrite scene values in actuator during download”, the scene values saved in the device will be overwritten with your preset values on downloading.

If you do not want to overwrite the values in the device when downloading, you must disable the parameter. In this case, the parameterized scene values are only written to the device memory during the first download.

If an application download is then carried out, the scene values in the device memory are retained.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?