MTN6710-0102S / MTN6810-0102 / MTN6805-0008

Position after Calibration via Object

The height position after the reference movement can be defined using the parameter “Position after calibration via object”. If a movement is to be made to a “new position”, set the height and, in the case of blinds, also the opening angle of the slats, in the movement range form 0% to 100%.

If the channel receives an absolute positioning command during the reference movement, it sets the desired position after the reference movement. In this case, the settings in the parameter “Position after reference movement via object” have no effect. All other control commands interrupt the calibrating function. The drive reacts to the received control commands.

Ext. 1/2

Output 1+2 / 3+4 / 5+6 / 7+8

-Blind/roller shutter

Calibration

-Automatic, Locking & Calibration settings

Position after calibration via object

Position prior reference movement

Remain in reference position

New position

   

Height position after calibration in %

0 (0-100)

   

Slat position after calibration in %

0 (0-100)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?