MTN6710-0102S / MTN6810-0102 / MTN6805-0008

Switching Cycle Counter

You can enable the Switching cycle counter counter function only for the switch/blind extension.

If you enable Switching cycle counter, all switching actions of a relay are counted and stored persistently in the memory. The actual value can be read for each relay via a 2-byte Switching cycle counter group object.

You have to enable the visibility of group objects in the Extended settings for your device. You can enable the visibility separately for each extension device.

Extended settings

Operating hours and switching cycle counter

 

Extension 1 switching cycle counter

Disabled/Enabled

 

Extension 2 switching cycle counter

Disabled/Enabled

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?