MTN6710-0102S / MTN6810-0102 / MTN6805-0008

Behavior of the Alarm after Bus Voltage Recovery

Disabled:
The alarm function is not activated after a bus voltage recovery, regardless of the state it had before the bus voltage failure.


Enabled:
After a bus voltage recovery, the alarm function becomes active and the output is switched to the state that you defined via the parameter Behavior at start of alarm.


As before bus voltage failure:
The alarm function is brought to the state that was active before the bus voltage failure. If the alarm function was active, the output is controlled by its settings in the parameter Behavior at start of alarm.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?