MTN6710-0102S / MTN6810-0102 / MTN6805-0008

Scenes

If you want to change multiple room functions simultaneously at the press of a button or with a command, you can do so using the scene function.

You can use a scene, for example, to switch on the room lighting, set the heating control to daytime operation and turn on the power supply for the sockets of a room.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?