MTN6710-0102S / MTN6810-0102 / MTN6805-0008

Automatic Load Detection (RC Mode/RL Mode)

In general, the connected loads are detected automatically for each channel. The load detection for each channel is performed as soon as the loads are connected and the mains voltage has been switched on.

The load is also checked with respect to inductive properties during continuous operation, and switched to RL operating mode if necessary.


NOTE: Loads may only be exchanged when the mains voltage is switched off.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?