MTN6710-0102S / MTN6810-0102 / MTN6805-0008

Operating Hours and Switching Cycle Counter

With the Operating hours and switching cycle counter function, you can turn on the counting of the operating hours of the dimmer master/extension and the number of switching cycles of the relay of the switch/blind actuator (if you choose switch/blind as one of the extensions).

You can enable/disable the counting function for each device separately.

If you enable Operating hours and switching cycle counter, group objects for this function appear in the newly created object folder Operating hours and switching cycle counter.

Extended settings

Operating hours and switching cycle counter

 

Master/Extension 1/2 operating hours

Disabled/Enabled

   

Extension 1/2 switching cycle counter

Disabled/Enabled

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?