Group Objects of the Express Setting Dimming
|
No. |
Name |
Object function |
Length |
Behavior |
Data Type |
|---|---|---|---|---|---|
|
55 |
Master Output 1 name of the channel |
Switch |
1 bit |
Received |
1.001 switch |
|
56 |
Master Output 1 name of the channel |
Dimming |
4 bits |
Received |
1.007 dimmer step |
|
57 |
Master Output 1 name of the channel |
Value |
1 byte |
Received |
5.001 Percent (0...100%) |
|
70 |
Master Output 1 name of the channel |
Feedback switch |
1 bit |
Sending |
1.001 switch |
|
71 |
Master Output 1 name of the channel |
Feedback value |
1 byte |
Sending |
5.001 Percent (0...100%) |
The dimming time for the respective function is preset and can be adjusted in the Extended settings for dimming(Dimming Times)
Moreover, two group objects are displayed for each output channel, reporting the current switching state and brightness value:
-
Status feedback switch object (1 bit) for the switching state feedback function
-
Status feedback value object (brightness value 1 byte) for the brightness value feedback function