Dimming Object Switches Channel
You can use the parameter Dimming object switches channel to determine the other functions of an output channel when a relative dimming telegram is received.
|
Master/Ext. 1/2 Output 1-2: Dimming |
Express settings for dimming |
||
|
Dimming object switches channel |
Not Only on Only Off On and Off |
||
Possible settings
-
Not
This parameter setting prevents switching on and off, for example, the channel remains off or at the minimum dimming value. -
Only On
The output channel can only be switched on by relative dimming telegrams. If it is switched on and the setpoint falls below A: Minimum brightness in % using relative dimming telegrams, the output remains switched on at the minimum dimming value. -
Only Off
The output channel cannot be switched on by relative dimming telegrams. If it is switched on and the setpoint falls below A: Minimum brightness in % using relative dimming telegrams, the output is switched off. -
On and Off
The output channel can only be switched on by relative dimming telegrams. If it is switched on and the setpoint falls below A: Minimum brightness in % using relative dimming telegrams, the output is switched off.