MTN6710-0102S / MTN6810-0102 / MTN6805-0008

Selection of the SpaceLogic KNX Extensions

The SpaceLogic KNX Dimmer Master is a KNX device to which you can connect two SpaceLogic KNX extensions.

You can choose one of the following extensions:

  • MTN6810-0102, SpaceLogic KNX Universal Dimming Extension

  • MTN6805-0008, SpaceLogic KNX Switch/Blind Extension

Master

Extension 1

Extension 2

Outputs

MTN6710-0102S

   

2 x dimming

MTN6710-0102S

MTN6810-0102

 

4 x dimming

MTN6710-0102S

MTN6810-0102

MTN6810-0102

6 x dimming

MTN6710-0102S

MTN6810-0102

MTN6805-0008

4 x dimming and
8 x switching or
4 x blind

MTN6710-0102S

MTN6805-0008

MTN6810-0102

4 x dimming and
8 x switching or
4 x blind

MTN6710-0102S

MTN6805-0008

MTN6805-0008

2 x dimming and
16 x switching or
8 x blind

The distribution of functions between channels is freely selectable and depends on your requirements.

General settings

SpaceLogic KNX Extension selection
 

Type of Extension 1

Disabled

MTN6810-0102 Universal Dimming

MTN6805-0008 Switch/Blind

 

Type of Extension 2

Disabled

MTN6810-0102 Universal Dimming

MTN6805-0008 Switch/Blind

Selecting MTN6810-0102 Universal Dimming adds Extension 1.

The 2 new dimming outputs with tabs, parameters, channels and channel functions are now available in the application.

Extension 1 is displayed as an image to the right of the master.

 

Selecting MTN6805-0008 Switch/Blind adds Extension 1.

The 8 new outputs with tabs, parameters, channels and channel functions are now available in the application.

Extension 1 is displayed as an image to the right of the master.

 

Selecting MTN6810-0102 Universal Dimming as Extension 2 adds the second dimming extension.

For Extension 2, the new outputs are now displayed with tabs, parameters, channels and channel functions.

Extension 2 is displayed as an image to the right of Extension 1.

 

Selecting MTN6805-0008 Switch/Blind as Extension 2 adds the second switch/blind extension.

For Extension 2, the new outputs are now displayed with tabs, parameters, channels and channel functions.

Extension 2 is displayed as an image to the right of Extension 1.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?