MTN6710-0102S / MTN6810-0102 / MTN6805-0008

Group Objects of Status Response of Automatic Mode

No.

Name

Object function

Length

Behavior

Data Type

160

Extension Output 1+2 name of the channel

Feedback for automatic mode

1 bit

Sending

1.003 Enable

The feedback object sends a "1" if automatic locking is active.

The feedback object sends a "0" if automatic locking is inactive.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?