MTN6710-0102S / MTN6810-0102 / MTN6805-0008

Express Settings for Roller Shutter

Roller shutter protects residents, furnishings and plants against too much sun and UV radiation. The roller shutter prevents the excessive heating of rooms from exposure to sunlight. The protection offered by roller shutters against external noise is also not to be underestimated.

In the cold season, the layer of air between window and shutter has an insulating effect. This can additionally save heating costs.

Roller shutters behave in a similar manner to blinds. They lack the slat control functions. For this reason, we refer to the description of the individual functions in the chapter Express Settings for Blind/Roller Shutter.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?