MTN6710-0102S / MTN6810-0102 / MTN6805-0008

Behavior of the Drive at Start of Locking

Set how the drive is to behave when the locking function becomes active:

  • No reaction: Finish the actual task.

  • Stop: The drive stops immediately (remains in its current position).

  • Up: The drive moves to the upper end position.

  • Down: The drive moves to the lower end position.

  • Move to position: The drive moves to the defined position for height and slat (for blind only).


Behavior at start of locking = move to position;
height position at start of locking = 40%; slat position at start of locking = 50%

Once the drive has performed the desired action, it remains in this position and cannot be operated while the locking function is active. Only when a function with a higher priority becomes active will the reaction defined there be executed.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?