MTN6710-0102S / MTN6810-0102 / MTN6805-0008

Off-delay

Master/Ext. 1/2 Output 1 – 2: Dimming

Off-delay time

Time settings

Off-delay time

Enabled

Disabled

   

Works on Switch object

Yes (Yes/No)

   

Works on Value object

Yes (Yes/No)

   

Works on Staircase object

No (Yes/No)

   

Works on Scene object

No (Yes/No)

   

Off-delay mode


Not retriggerable

Retriggerable

Retriggerable and adding

   

Max. number of additions

2 (2 – 5)

   

Off-delay time

1 s (0 ms – 1 h)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?