MTN6710-0102S / MTN6810-0102 / MTN6805-0008

Extended Settings for Switching

On the Express settings for switching tab, activate the Extended settings for switching.

Ext. 1/2 Output 1-8 -Switch: Switching

Express settings for switching

 

Extended settings for switching

Disable

Enable

– Time settings

Staircase lighting time

On-delay time

Off-delay time

– Logic, Locking & Priority settings

Priority function

 

Logic function

 

– Safety and alarm settings

Safety function

 

Alarm function

   

Failure and download behavior

 

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?