Automatic Mode
In addition to manual control of the blind / roller shutter drives (via the group objects for the manual operating options), the software application also provides you with another set of group objects for automatic control.
Automatic control can be performed by other bus devices, e.g. presence detectors or light controllers, or via a building control system. Once you have activated automatic control for a channel, you can initially position the connected drive with equal priority using manual control or automatic control. The drive reacts identically on receiving control telegrams from one of the two types of control.
|
Ext. 1/2 Output 1+2 / 3+4 / 5+6 / 7+8 -Blind/roller shutter |
Automatic, Locking & Calibration settings |
||
|
-Automatic, Locking & Calibration settings |
Automatic mode |
||
|
Automatic mode |
Disabled Enabled |
||
In order to use the automatic mode, you must first activate the function in the ETS. Once automatic mode has been enabled, new group objects are available for the channel.