MTN6710-0102S / MTN6810-0102 / MTN6805-0008

Deceleration Delay

There are some motors that continue running for several milliseconds after they are switched off. This can also be caused by large and heavy blinds/roller shutters. If you notice this behavior, you can compensate for it using the setting for the deceleration delay.

A value = 6 gives a deceleration delay of 6 x 10 ms = 60 ms.

In this way, the motor will be switched off 60 ms earlier.

Ext. 1/2

Output 1+2 / 3+4 / 5+6 / 7+8

-Blind/roller shutter

Extended drive timing

-Extended drive timing

Deceleration delay (0...255, unit = 10 ms)

0

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?