MTN6710-0102S / MTN6810-0102 / MTN6805-0008

Same Dimming Time for Central Function and Scenes

In the global (extended) settings, you can activate the same dimming time for central function and scenes. (Same Dimming Time at Central Function and Scenes).

After general activation of the same dimming time, you can link the scene function of an output channel with this function.

Master/Ext. 1/2 Output 1 – 2: Dimming

Scene settings

 
Scenes settings

Same dimming time

Disabled

Enabled

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?