MTN6710-0102S / MTN6810-0102 / MTN6805-0008

Priority

The reaction to the behavior set here for bus voltage recovery has a low priority. If a function with a higher priority is activated for the switching channel directly after bus voltage recovery, the settings described below apply to these functions.

Relay states caused by higher-priority functions (higher-level function) take precedence over behavior after bus voltage recovery.


Example:

OR logic operation with parametrized value of the logic object after bus voltage recovery = 1, prevails and switches the output.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?