MTN6710-0102S / MTN6810-0102 / MTN6805-0008

Roller Shutter

To control roller shutter, you can switch the channel function of the device to Roller shutter mode.

General settings

Channel function Extension 1 / Extension 2 Output 1-8 Roller shutter
   

Ext. 1/2
Output 1+2; 3+4; 5+6; 7+8: Roller shutter

Express settings for Roller shutter

...

Express Settings for Roller Shutter

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?