MTN6710-0102S / MTN6810-0102 / MTN6805-0008

Staircase Lighting Time Function in Combination with On-delay and Off-delay

Combining a staircase lighting time function with an on-delay results in a delayed start of the staircase lighting function.

The result of combining a staircase lighting time function with an off-delay depends on how you have defined the staircase lighting time function:

In the case of the staircase lighting time function with manual switching off (“0” telegram), the off-delay is started if a premature switch-off telegram is received on the “staircase lighting time object”. Once the off-delay time has elapsed, the output is switched off.

In the case of the staircase lighting time function without manual switching off, receipt of a switch-off telegram on the “staircase lighting time object” has no effect. The staircase lighting time function continues to the end and then switches off the output. An off-delay cannot be set.


Staircase lighting time function with off-delay

For staircase lighting time functions with manual switching off and warnings activated, the staircase lighting time function is immediately deactivated with a warning when an “Off” telegram is received. The off-delay elapses. No warning is generated.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?