Group Objects for Dimming Time for Scenes and Central Function
|
No. |
Name |
Object function |
Length |
Behavior |
Data Type |
|---|---|---|---|---|---|
|
8 |
Central |
Dimming time for scenes and central |
2 bytes |
Received |
7.004 time (100 ms) |
With a telegram, the same dimming time for scenes and central function can be set or modified via the object (2 byte DPT 7.004 time (100 ms)) between 0 ms and 99:59:9 ms, e.g., using a button. This allows you to specify the length of the dimming time from different places according to the desired situation.