MTN6710-0102S / MTN6810-0102 / MTN6805-0008

Switch Object Behavior

You can define the behavior of the switch object for each channel.

Master/Ext. 1/2 Output 1-2: Dimming

Express settings for dimming

 

Switch object behavior

Normal

Inverted

It can be operated normally or inverted.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?