MTN6710-0102S / MTN6810-0102 / MTN6805-0008

Name of the Channel Dimming

You can assign a separate name for each channel, e.g. “Light Hall Ground Floor”. This individual name is appended to the fixed channel name, e.g. “Master Output 1 - Dimming”. The full name of the channel is then, e.g. “Master Output 1 – Dimming Light Hall Ground Floor”.

The name of the channel now appears on the parameters, channels and associated group objects.

Master/Ext. 1/2 Output 1-2: Dimming

Express settings for dimming

 

Name of the channel

Light Hall Ground Floor

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?